Specify the Gauge Off Time

Use the Gauge Off Time field on the Lufkin SAMS tab to define the start of the working day. The property also defines the time at which ClearSCADA updates the following point values in the database:

Either use the spin box to select the required time, or overtype the entry (remembering to use 24-hour clock settings).



Disclaimer

ClearSCADA 2017 R2