Displaying a ClearSCADA Map

You can create single-layer maps or multi-layer composite maps in ClearSCADA, from online or offline mapping sources, which you can then use for a variety of purposes. For example, you can display:

Once you have created a map in ClearSCADA (see Creating a ClearSCADA Map), you can display it as follows:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, either double-click on the Map Source or Map Set database item that represents the map you want to display, or right-click on the item. If you double-click, ClearSCADA will then display the map. If you right-click, ClearSCADA will display the Object menu. Select the Display Map Set or Display Map Source option as appropriate. ClearSCADA will then display the map.

Display the Geographic Location of a Database Item

You can display the geographic location of a database item on a ClearSCADA map (see Displaying the Geographic Location of a Database Item).

Display a Map in a Mimic

You can also display a map in a mimic. For more information, see Creating a Hyperlink to a Map in the ClearSCADA Guide to Mimics.


Disclaimer

ClearSCADA 2017 R2