Animating an Object to Trigger a System Command

You can animate an object so that when it is selected, it causes a Windows system command to be executed. Common uses for this type of animation include:

(Although both of these can also be set up by using the Pick Action Wizard, see Creating a System Command Pick Action).

When animating an object to trigger a system command, you need to set the PickType to 16 (for System command). You also need to define the system command (or the location of a System Command database item) in the PickParam expression.

Example:

A Mimic object that is configured to run Internet Explorer when selected could have these animations:

  • PickType—16
  • PickParam—'C:\Program Files\Internet Explorer\iexplore.exe'

    The same functionality could be provided by configuring a System Command item to have the Command: 'C:\Program Files\Internet Explorer\iexplore.exe'. Next, you would configure a Mimic object to use the following animations:

  • PickType—16
  • PickParam—"<location of System Command item>.cmd"

    Where <location of System Command item> is a reference to the System Command item. The PickParam has to reference the System Command item’s cmd property.


Disclaimer

ClearSCADA 2017 R2