Animations

Each Mimic object has properties that you can associate with values in the database. For example, you can associate the size of a Mimic object with the value of an analog point so that the Mimic object is larger when the point has a high value.

Associating the property of a Mimic object with the property of an item in the database is referred to as animating an object.

You can also use an animation to associate a Mimic object property with a specific value. For example, you can associate the FillColour property of a text box with an RGB value so that the FillColour is set to a specific color.

By configuring animations, you can allow Mimics to:

By using the animations feature, you can create Mimics that provide the information and interactivity required by operators.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R2