BackAlpha

The BackAlpha property works in a similar way to FillAlpha property, except that instead of representing the amount of transparency for the fill, it represents the amount of transparency that is applied to the background of an embedded Trend, X-Y Plot, or X-Y-Z Plot.


Disclaimer

ClearSCADA 2017 R2