Blink

The Blink property is used to define whether the flash feature is on or off for the line/outline.

The Blink property for lines works in exactly the same way as the Blink property in the Fill group except that it applies to the line/outline. For more information, refer to the Fill Animations section (see Blink).


Disclaimer

ClearSCADA 2017 R2