Define the Grid Settings for a Mimic

You can use the Mimic Properties window to define whether a Mimic has its Grid enabled or disabled. When the Grid feature is enabled, all objects on a Mimic are aligned with a grid line automatically. This alignment is referred to as an object being 'snapped to grid'.

Depending on the method that you use to display the Mimic Properties window, the settings you define will be applied to:

When you have displayed the Mimic Properties window using the appropriate method for your needs, define the Grid settings as follows:

You can also toggle the grid on and off by using the Grid command in the Arrange command group on the Graphics Tab.


Disclaimer

ClearSCADA 2017 R2