Define the Magnification Settings for a Mimic

You can use the Mimic Properties window to define whether a Mimic can have its level of magnification altered in Run Mode and also the range of magnification permitted. This is useful when you need to restrict access to certain levels of magnification or wish to disable magnification in Run Mode to simplify the level of user interaction with a Mimic.

Depending on the method that you use to display the Mimic Properties window, the settings you define will be applied to:

When you have displayed the Mimic Properties window using the appropriate method for your needs, define the magnification settings as follows:

Further Information

Magnifying a Mimic (Zooming)

Displaying a Mimic

Run Mode and Design Mode.


Disclaimer

ClearSCADA 2017 R2