Define the Polyline Line Settings for a Mimic

You can use the Polyline Line tab of the Mimic Properties window to define the default settings for lines that are drawn on Mimics. This is useful when you know that many different lines of the same type and style need to be added to a Mimic. Rather than configure each line separately, you can define the default settings for lines—then every line that is added will already have the default settings in place. You can make further adjustments to each line by configuring its own settings separately if required.

Depending on the method that you use to display the Mimic Properties window, the settings you define will be applied to:

When you have displayed the Mimic Properties window using the appropriate method for your needs, define the Polyline Line settings as required. The various PolyLine Line settings work in the same way as the similarly named settings on the Line tab of the Polyline Properties window (see Editing a Line).


Disclaimer

ClearSCADA 2017 R2