FlashOffset

The FlashOffset works in exactly the same way as the FlashOffset property in the Fill group except that it applies to the flash sequence for the line/outline rather than the fill. Typically, you would set the flash offset on the Polyline Properties window (it is not designed to be used as an animation).


Disclaimer

ClearSCADA 2017 R2