GradAlpha

The GradAlpha property defines the amount of transparency that is applied to the GradColour. This works in exactly the same way as the FillAlpha property, except that it applies to the secondary color that is used in the Linear Gradient, Pipe Gradient, or Radial Gradient shading.


Disclaimer

ClearSCADA 2017 R2