Using Drag and Drop to Create a Hyperlink
You can use Windows' Drag and Drop functionality to add a new hyperlink to a Mimic. Creating a hyperlink in this way adds a new text box to the Mimic—the text box is automatically configured to hyperlink to another display.
You can use drag and drop to automatically configure a hyperlink for an existing Mimic object or a new text box. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.