Using the Animations Window

When you have displayed the Animations window, you can use it to view, edit, remove, and create animations. Each animation either defines a value for a particular setting or associates an animation property with one of the properties of a database item.

The animation properties are listed in the main display. They are listed in a tree-structure, with sets of related animation properties being grouped in branches. You can expand any branch by selecting the + icon.

The following information is provided (where applicable):

The Animations window also has these buttons:

For information on the animation properties, see Understanding the Animation Properties.


Disclaimer

ClearSCADA 2017 R2