Configure the Scanner Properties

Use the fields on the Scanner tab of the Mitsubishi Scanner Form to define the general and Mitsubishi-specific properties for a scanner. Many of the fields on this tab are common to many scanners (see Configuring Scanners on Simple Drivers in the ClearSCADA Guide to Simple Drivers). Those fields that are specific to scanners on the Mitsubishi driver are described below.

For further examples showing how you might configure the Device, Data Address, and Data Length properties, see Configuration Examples.


Disclaimer

ClearSCADA 2017 R2