Points Used on Mitsubishi Scanners

Mitsubishi Scanners can support analog points and digital points.

You configure the Mitsubishi points on your system by using the appropriate Mitsubishi Point Form. The Forms have several tabs (see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers).

For information on configuring properties on the Mitsubishi tab, see Configuring Analog Points, or see Configuring Digital Points, as appropriate.

For information on configuring properties on the <Point Type> tab, see the appropriate reference below:

For fields on the other tabs, see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers.

For general information on creating a point and displaying a Point Form, see Configuring a Point in the ClearSCADA Guide to Core Point Configuration.


Disclaimer

ClearSCADA 2017 R2