Modbus Master Communicating with one or more Modbus Devices

Where ClearSCADA retrieves data from Modbus PLCs, or third-party devices that are communicating using the Modbus protocol, the ClearSCADA system acts as a Modbus Master.

For this scenario, the Simple Modbus driver has to be running on your system, and you need to configure the required number of Modbus channels, Modbus scanners, and Modbus points within ClearSCADA.

For further information, see Configuring Modbus Devices in ClearSCADA.


Disclaimer

ClearSCADA 2017 R2