Secondary Assign

Associated with: Channels on the Simple Modbus driver

This attribute indicates whether the assignment of a channel to its secondary line has failed. The line is that which is defined on the Secondary tab of the Channel Form.

Possible states: Displays one of the Standard Alarm States.


Disclaimer

ClearSCADA 2017 R2