Switch Line

Associated with: Simple Modbus channels that can use either of two lines

Security permission required to access this pick action: Switch Line

If communications on one line fail, a Modbus channel automatically switches to use the other line. If communications on both lines fail, automatic switching ceases until communications recover. You can use the Switch Line pick action to force line switching to continue, or force the channel to use a particular line.

When you select the Switch Line pick action, the Switch Line window is displayed.

Use the combo box to select the required type of switching.

Choose from:


Disclaimer

ClearSCADA 2017 R2