Connection Properties

Use the Connection Type field on a Modbus Slave Channel’s Connection tab to specify the type of channel connection that is to be used.

Modbus Slave channels are able to communicate using either Serial or TCP/IP connection, depending on your system setup.

For information on configuring a Serial connection, see Configure a Channel’s Serial Connection Properties in the ClearSCADA Guide to Drivers.

For information on configuring a TCP/IP connection, see Configure a Modbus Slave Channel’s TCP/IP Connection Properties.


Disclaimer

ClearSCADA 2017 R2