Configuring Digital Points
NTP Monitor Scanners support digital input points.
You need to configure one digital point in the ClearSCADA database for each point that monitors digital-type data on an NTP device.
Configure the digital point’s properties using the fields on the NTP Monitor Digital Point Form.
The Form has several tabs.
The fields on the Digital Point tab are common to digital points on many drivers (see Defining Digital Point Details in the ClearSCADA Guide to Core Point Configuration).
Use the fields on the NTP Monitor tab to Configure the NTP Monitor Point Properties.
For information on the fields on other tabs, see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers.