Configuring Time Points

Use Simple OPC Time points to map time values on OPC servers into ClearSCADA.

Configure the properties of each Time point using the fields on the Simple OPC Time Point Form.

For information the Time Point tab on the Time Point Form, see Defining Time Point Details in the ClearSCADA Guide to Core Point Configuration.

For information on the Control tab, see Define the Control Settings for a Time Point in the ClearSCADA Guide to Core Point Configuration.

For information on the fields on the OPC tab, see Configure General Properties on the OPC Tab, and see Specify the Source Value of a Point.

For information on the fields on other tabs, see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers.


Disclaimer

ClearSCADA 2017 R2