Configure the Scanner Properties

Use the fields on the Scanner tab to define the driver-specific properties of a scanner. Some of these fields are common to many scanners (see Configuring Scanners on Simple Drivers in the ClearSCADA Guide to Simple Drivers). Those fields that are specific to scanners on the OPC XML-DA Client driver are described below.


Disclaimer

ClearSCADA 2017 R2