Configure an SMS Pager Service

If you are using a GSM modem to send SMS messages to pager devices or mobile telephones, you need to configure SMS Pager Service database items to represent the SMS protocol.

For each GSM modem that you are going to use, you will need to configure one SMS Pager Service and one SMS Pager Channel.

To configure an SMS Pager Service:

  1. Log on to your system via a User Account that has the Configure Database permission (see Allocating Security Permissions in the ClearSCADA Guide to Security).
  2. Display the Pager Service Form for the Pager Service item you want to configure. If the item does not already exist in the database, you will need to Create a Pager Service Database Item.
  3. Configure the properties on the Identification, User Methods, Alarm, and Redirection tabs as required (see Tabs on Configuration Forms).
  4. Select the SMS Service tab.
  5. Configure the 'common' Pager Service properties on the tab (see Configure the Common Pager Service Properties).
  6. Define whether an SMS Service can Process Incoming Messages.
  7. Define the Number of Times an SMS Service will attempt to Process Messages.
  8. Define how the Modem Should Process Incoming SMS Messages.
  9. Define whether ClearSCADA Replies to Incoming SMS Messages.
  10. Define the Data Coding Scheme for an SMS Service
  11. Save the configuration (see Saving Configuration Changes in the ClearSCADA Guide to Core Configuration).

Further Information

Configure an SMS Pager Channel.


Disclaimer

ClearSCADA 2017 R2