Preparation

Before you can successfully configure a Pager Channel, you need to configure an appropriate Pager Service (see Configuring a Pager Service). For example, can only configure a PSTN Pager Channel if you database already has a suitably configured TAP or UCP Pager Service.

During the configuration of your Pager Channel, you may also need to know:

When you have configured Pager Services and Pager Channels, you will need to define Pager Contact information in the User accounts of each user that is to receive pager or mobile telephone messages from ClearSCADA.


Disclaimer

ClearSCADA 2017 R2