Using SMS to Trigger an Action

By using an SMS service and SMS channel, you can instruct ClearSCADA to perform actions remotely. This means that engineers and operators can use SMS compatible devices such as mobile telephones to trigger actions in ClearSCADA from any location that has suitable network coverage.

There are three ways of sending an SMS message to trigger an action:

We recommend that wherever possible, you use an alias on a Method Call. This is because this way of sending an SMS command is much more convenient, cost-efficient and reliable. To learn how to use an alias on a Method Call, see:

If, for some reason, you need to use a different technique for issuing an SMS command, please refer to the following sections:


Disclaimer

ClearSCADA 2017 R2