Disconnect QueryPad from a Database

Once connected to a database, QueryPad uses a heartbeat feature to remain active - a heartbeat signal is sent via the connection every hour. This means that QueryPad’s connection to the server will be closed if:

When you have finished using QueryPad, you should disconnect it from the database to which it is connected.

To disconnect QueryPad from a database:


Disclaimer

ClearSCADA 2017 R2