DailyHistory Mimic

The Mimics group in the ROCPlusDemo.sde contains a DailyHistory Mimic.

The Mimic displays the daily history values, along with timestamps and a quality description for all four runs from the ROC. Click on any value to display the underlying point’s object menu. You can use the menu options to view a historic list or a historic Trend to verify that the data was retrieved from the flow computer correctly.

You can exercise the driver by clicking a value, opening that point’s property menu, disabling history, verifying that the history is deleted, and then re-enabling history on the point. The driver will backfill the point data from the flow computer.


Disclaimer

ClearSCADA 2017 R2