How can I change the orifice plate diameter for a flow run?

To read the orifice plate diameter, set up a ROC Plus Numeric Point to read from Type = 113, Location = Run number – 1 and Parameter = 15. Enable the Control aggregate on the point. To change the value, call the Control method on the Control aggregate for the point.

For further information, see ROC Plus Numeric Point.


Disclaimer

ClearSCADA 2017 R2