How can I change the pipe material for a flow run?

To read the pipe material, set up a ROC Numeric Point to read from Type = 113, Location = Run Number – 1 and Parameter = 14. You will need to decode the value that is read manually.

To change the pipe material, make sure the Control aggregate is enabled and then call the Control method on the Control aggregate with an appropriate parameter.

For further information, see ROC Plus Numeric Point.


Disclaimer

ClearSCADA 2017 R2