How long does the driver hold a TCP/IP connection open?

The driver task will hold a TCP/IP connection to a ROC open for the number of seconds specified in the TcpConnectionTimeout field on the ROC Plus Channel object. Any communication with a ROC over an existing socket, including demand polls and control requests, cause the timeout to be reset.

For further information, see ROC Plus Channel.


Disclaimer

ClearSCADA 2017 R2