Device Point Mapping
Associated with: SCADAPack 50 Points and SCADAPack 50 Outstations.
For points, this status attribute shows the device point (V1-V8) to which a ClearSCADA point maps, as shown in the illustration below:
For outstations, the Status display shows this information for each device point that is mapped to a ClearSCADA point. There is one Device Point Mapping attribute line for every mapped point, as shown in the illustration below:
When you make a change to a device point's mapping in ClearSCADA, ClearSCADA will display a Device Point Mapping message in the Outstation Status window. An example is shown in the illustration below:
For more about mapping device points, see Map ClearSCADA Points to SCADAPack 50 Device Logical Points.