Diagnostic Measure Config

Associated with: SCADAPack 50 Outstations.

This status attribute shows a derived estimate of the total amount of energy consumed by the device (in microamps x 100) since the device was first activated. The device calculates this measure by using the Power Gauge value (see Specify the Device Configuration System Options). You can use this energy consumption measure to predict how long the battery will last. For more information, see the SCADAPack 50 device documentation.

NOTE: This attribute indicates the latest value that the device has sent to ClearSCADA. The device transmits the data to ClearSCADA in diagnostic SMS messages.


Disclaimer

ClearSCADA 2017 R2