Enable Configuration Download
Use the Configuration Download Enabled check box on the SCADAPack 50 tab to enable users to send a configuration from ClearSCADA to a device.
- Configuration Download Enabled—Select this check box to enable users to send a configuration from ClearSCADA to a device. Clear this check box to help prevent users from being able to send a configuration.
If the check box is clear, then ClearSCADA 'grays out' the configuration-related fields on this tab because they are not applicable.