Retrieve Diagnostics

Associated with: SCADAPack 50 Outstations.

Security permission required to access this pick action: Retrieve Data.

Use this pick action to instruct the device to send diagnostic information to ClearSCADA. The device will not receive the action request until it has sent at least one more set of data SMS messages. Therefore, the action will not take place immediately.

Select the Retrieve Diagnostics pick action to display the Retrieve Diagnostics window.

Select the OK button to confirm your selection.

If you are using this pick action with the Automation Interface, you need to specify the method name RetrieveDiagnostics.


Disclaimer

ClearSCADA 2017 R2