Specify an Outstation Telephone Number

Use the Telephone Number property on the SCADAPack 50 tab to specify the telephone number of the device modem. ClearSCADA can potentially receive messages from many devices. The Telephone Number and Outstation Name together identify to ClearSCADA which device this is (see Specify an Outstation Name).


Disclaimer

ClearSCADA 2017 R2