Specify the ClearSCADA Port for the GSM Modem

Use the Port field on the Connection tab to specify the ClearSCADA COM port to which the ClearSCADA GSM modem is connected (see Configure a Channel's Serial Connection Properties in the ClearSCADA Guide to Drivers).


Disclaimer

ClearSCADA 2017 R2