Modbus Function Codes Supported by the ClearSCADA SCADAPack Modbus Driver

The ClearSCADA SCADAPack Modbus Driver supports several Modbus function codes, enabling it to read and write data on SCADAPack devices. The standard function codes that the ClearSCADA SCADAPack Modbus Driver supports are the same as those that are supported by its 'parent' Advanced Modbus driver (see Modbus Function Codes Supported by the ClearSCADA Advanced Modbus Driver in the ClearSCADA Guide to the Advanced Modbus Driver):

For information on the controller address ranges that apply to the different types of Modbus data, see SCADAPack Point Addressing.

In addition to the above standard function codes, the ClearSCADA SCADAPack Modbus Driver also supports a number of proprietary function codes. These codes are used with SCADAPack controllers.


Disclaimer

ClearSCADA 2017 R2