Polling Suspended

Associated with: SCADAPack controllers

This attribute indicates whether polling of a controller is presently suspended. Polling can be suspended and resumed automatically, using the Remote Connection interface. On controllers on which the ‘Suspend Polling’ feature is enabled, polling can also be suspended and resumed by using the Suspend Polling and Resume Polling pick actions, respectively.

Possible states: True, False


Disclaimer

ClearSCADA 2017 R2