Compressibility Calculation Error Code
Associated with: Flow runs
This attribute indicates whether the Flow Run’s Compressibility Calculation has generated an error. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller. Information is displayed in this format:
<Error Code>:<Description>
where 0: No error indicates that the calculation has recalculated successfully. If an error has occurred, a 5-digit error code and corresponding description is displayed.
Example:
20002: Inputs have not been configured
For a list of compressibility calculation error codes and their corresponding descriptions, see the documentation provided with the Realflo application.