Configure ClearSCADA to Monitor Realflo Calculation Data

On a ClearSCADA system, you configure the ClearSCADA database so that entries in the database correspond to the plant, measuring instruments, and control devices on your system. This section summarizes the database items that you need to configure to represent the SCADAPack Modbus Realflo devices on your system.

In order to represent any SCADAPack Modbus Realflo devices, both the SCADAPack Modbus Driver and the Realflo extension component have to be installed and running on the ClearSCADA servers on your system (see Confirm that the Realflo Server Component is Installed). When the driver is first installed, a system administrator needs to define the server settings for the driver (see Configuring SCADAPack Modbus Server Settings in the ClearSCADA Guide to the SCADAPack Modbus Driver, and see Configuring Realflo Server Settings in this guide).

When you configure SCADAPack Modbus Realflo items in the ClearSCADA database, many of the settings for those items need to correspond to the settings of the relevant SCADAPack Modbus Realflo devices on your system. Some settings are either fixed (incorporated into the design of the Realflo-enabled SCADAPack controller), or are configured by an engineer. You need to have access to, or an understanding of, the settings of the SCADAPack Modbus Realflo devices on your system before you can configure the SCADAPack Modbus Realflo database items successfully. For instance, you need to specify the user ID and passcode needed to access the Realflo components on each Realflo-enabled SCADAPack controller on your system.

You also need to be aware of which optional features are required for each SCADAPack Modbus Realflo item. These features include:

You can also use core ClearSCADA features with SCADAPack Modbus Realflo database items, including Lists, Actions, and Mimics. For actions that are specific to the SCADAPack Modbus driver, see Using SCADAPack Modbus Specific Actions in the ClearSCADA Guide to the SCADAPack Modbus Driver, and see Using Realflo Specific Actions in this guide. For further information on actions and for details on Lists and Mimics, see the core documentation.

In order for ClearSCADA to monitor flow data via SCADAPack devices that are running Realflo, you need to configure:

If you want other applications to communicate remotely with SCADAPack Modbus Realflo devices via ClearSCADA, you also need to configure a Remote Connection.

see Configuring an Advanced Modbus Remote Connection in the ClearSCADA Guide to the Advanced Modbus Driver.

To minimize the time that it takes to configure the required SCADAPack Modbus Realflo items, you may want to configure them in the order listed above, as set configuration requires you to specify a channel, and controller (outstation) configuration requires you to specify a set, and so on.

Realflo-enabled SCADAPack controllers only support writing of Flow Run configuration from the ClearSCADA server. However, you may be able to write other configuration remotely, via applications such as Telepace®. Refer to the documentation supplied with the application for information.

Be aware that some of the configuration properties, features and functionality mentioned in this guide are only supported by particular versions of Realflo firmware onwards. As such, not all of the properties and features described in this guide might be available on, or supported by, the Realflo devices on your system.


Disclaimer

ClearSCADA 2017 R2