Current Data Last Updated

Associated with: Flow runs

This attribute indicates the date and time that ClearSCADA last updated the Flow Run’s current data. ClearSCADA applies the time stamp when it updates the data in its database. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller.

Example:

07/Jun/2012  08:42:00.314


Disclaimer

ClearSCADA 2017 R2