Differential Pressure Alarm

Associated with: Flow runs

This attribute indicates that the Differential Pressure is in alarm and displays the value of that Differential Pressure. The attribute is displayed once the Instantaneous and Accumulated Readings Registers are read from the Flow Computer. The units that apply to the attribute depend on the Measurement Units system being used for the Flow Run’s Contract Units.

Example:

9.065
(for a value in kPa)


Disclaimer

ClearSCADA 2017 R2