Event Log Demand Poll
Associated with: SCADAPack Modbus Flow Runs
Security permission required to access this pick action: Retrieve Data
Use this pick action to request the driver to perform an Event Log Demand Poll on a controller for the events that are associated with a particular Flow Run.
- Select the Event Log Demand Poll pick action to display the Event Log Demand Poll window.
- Use the window’s Range field to specify which events to retrieve:
- New—Retrieve only those events that have been raised since the last Event Log Demand Poll.
- All—Retrieve all of the Flow Run’s events from the controller’s event log.
Retrieving All of a Flow Run’s events may result in duplicate entries being logged in ClearSCADA ’s Event Journal.