Execution State
Associated with: Flow runs
This attribute indicates the present execution state of the Flow Run’s calculations. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller.
Possible States:
- Not Set
(The Flow Run has never executed. This state typically applies to newly configured Flow Runs that have not yet been put into service.) - Stopped
(The Flow Run’s calculations have stopped running in the Gas Flow Computer.) - Running
(The Flow Run’s calculations are running at the Gas Flow Computer, and the Flow Run’s current readings are being updated.)