Gas Flow Application Number

Associated with: Realflo controllers

This attribute indicates the version of the Gas Flow application that is running on the controller. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller.

Example:

6.01


Disclaimer

ClearSCADA 2017 R2