Liquids Properties (Liquid Flow Run)

The fields within this section of the Liquid tab display those properties that are associated with Liquids measurement.

You can configure these properties directly in ClearSCADA, or read the configuration into the ClearSCADA database (see Configure or Read the Flow Run Configuration).

Further Information

For more detailed information on these properties, see the documentation provided with the Realflo application.


Disclaimer

ClearSCADA 2017 R2