Realflo Specific Status Display Attributes

This driver is an extension driver. As such, it supports a combination of the status attributes that are supported by its 'parent' driver, in addition to its own driver-specific status attributes. Use this section in conjunction with the 'parent' driver documentation for comprehensive information about the status attributes that are supported by this extension driver.

The topics in this section explain those status attributes that are SCADAPack Modbus Realflo-specific. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Further Information

Status attributes supported by this driver's parent driver: see SCADAPack Modbus Specific Status Display Attributes in the ClearSCADAGuide to the SCADAPack Modbus Driver.


Disclaimer

ClearSCADA 2017 R2