SCADAPack Modbus Realflo Point Addressing

Controllers on the SCADAPack Modbus driver support one of two point address ranges—5 Digit, or 6 Digit. You need to be aware of which address range each controller on your system supports. (For instance, current SCADAPack controllers use 5-Digit addressing.) Specify the supported Point Address Range on each SCADAPack Modbus Realflo Outstation Form (see Specify the Point Address Range in the ClearSCADA Guide to the Advanced Modbus Driver).

ClearSCADA assigns Realflo Analog Input point addresses automatically. However, you still need to manually assign appropriate addresses for those SCADAPack Modbus points that represent data other than Realflo data on a Realflo controller. For such points, specify the individual point Address on each SCADAPack Modbus Point Form (see Configure Common Point Properties in the ClearSCADA Guide to the SCADAPack Modbus Driver).

Further Information

SCADAPack Modbus Point Addressing in the ClearSCADA Guide to the SCADAPack Modbus Driver.


Disclaimer

ClearSCADA 2017 R2