Source (Liquid Flow Run)

Associated with: SCADAPack Modbus Realflo Outsations, and SCADAPack Modbus Realflo Analog Input points

The Source attribute is common to many Status displays. The attribute indicates the location at which an item resides. The information shown varies, depending on the type of item.

For SCADAPack Modbus Realflo Outstations, the attribute displays information in this format:

Set <Set Address>:OS <Controller Address>

For SCADAPack Modbus Realflo Analog Inputs, the attribute displays information in this format:

Set <Set Address>:OS <Controller Address>:Flow Run <Flow Run Number>:AI Source <Source Number>:Item <Item Number> (Address <Point Address>)

where:

For information about either of the above properties, see Configure the General Realflo Analog Point Properties.

The table below indicates the type of Flow Run Source <Source Number > represents.

Source Number Source Type
0 Accumulation
1 Input
2 Flow Calculation
3 Compressibility Calculation
4 Density Calculation
10 Daily Flow History
11 Hourly History Data
12 Batch Records Data

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Accumulation (<Source Number>=0).

Item Number Liquid Flow Run Data Item Type
3 Net standard volume: water during previous contract day (Liquid only)
4 Average CPLo during previous contract day (Liquid only)
5 Number of flow calculations during contract day
6 Duration of flow during contract day
7 Gross Standard Volume at base conditions during contract day (Liquids only)
8 Net standard volume: oil during contract day (Liquid only)
9 Average CTL: oil during contract day (Liquid only)
10 Total accumulated GSV: oil at base conditions (Liquid only)
11 Flow duration in current month
12 GSV: oil during current month
13 Flow duration in previous month
14 GSV: oil in previous month
15 Duration of flow during previous contract day
16 GSV at base conditions during previous day
17 Net standard volume: oil during previous contract day
18 Average CTL: oil during previous contract day
19 Number of flow calculations during previous contract day
20 Average CPLo during the contract day (liquid only)
21 Average Temperature correction factor: oil CTLo
22 Net standard volume: Water during contract day
23 Average temp correction factor: water CTLw current day (Liquids only)
24 Average temperature correction factor: water CTLw during previous day
25 Net Standard Volume: oil during the current month (Liquid only)
26 Net Standard Volume: oil during the previous month (Liquid only)
27 Total accumulated net standard flow volume (Liquid/water only)
28 Net standard volume: water during the current month (Water only)
29 Net standard volume: water during the previous month (Water only)

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Input (<Source Number>=1).

Item Number Liquid Flow Run Data Item Type
1 Calibration flags
2 Temperature Input Alarm
3 Static Pressure Input Alarm
4 Mass Pulse (AGA-11/Liquid/Water) Input Alarm
4 Live turbine meter pulses (AGA-7 or Mass/Volume Pulse AGA-11/Liquid/Water)
6 Live Temperature
7 Live Static Pressure
8 Live Mass flow (AGA-11/Liquid/Water)
9 Forced Temperature
10 Forced Static Pressure
11 Forced Mass Flow (AGA-11/Liquid/Waters)
12 Forced Pulse Rate (AGA-7 or Mass/Volume Pulse AGA-11/Liquid/Water)
13 Current turbine meter pulses (AGA-7 Gas or Mass/Volume Pulse AGA-11/Liquid/Water)
14 Current Mass Flow (AGA-11/Liquid/Water)
15 Current Density
16 Current Water Cut
17 Current Input Temperature
18 Current Static Pressure
19 Density Input Alarm
20 Water Cut Input Alarm
21 Live Density
22 Live Water Cut
23 Forced Density
24 Forced Water Cut

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Flow Calculation (<Source Number>=2).

Item Number Liquid Flow Run Data Item Type
1 Compressibility approximated flag
2 Input or flow calculation error code
3 Flow volume rate
4 Flow mass rate
5 Base Density (Liquids only)
7 Date of Flow Update
8 Time of Flow Update
9 Current pressure correction factor: oil CTLo (Liquid only)
10 Total Two-phase flow time
11 Maximum Two-phase duration

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Daily Flow History (<Source Number>=10), or Hourly History Data (<Source Number>=11).

Item Number Liquid Flow Run Data Item Type
1 Duration of Flow in Period
2 Net Standard Volume Oil
3 Net Standard Volume Water
4 Indicated Volume
5 Gross Standard Volume
6 Average Temperature
7 Average Static Pressure
8 Average Density
10 S & W Factor
11 Input Units
12 Contract Units
13 Number of Alarms
14 Number of Events
15 Meter Factor
16 K Factor
17 Meter Input Type
18 Average T correction (CTL) Oil
19 Average T correction (CTL) Water
20 Average P correction (CPL)
21 User Data 1
22 User Data 2
23 User Data 3
24 User Data 4
25 User Data 5
26 Batch ID
27 Duration of period
28 QTR Identifier

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Batch Records (<Source Number>=12).

Item Number Liquid Flow Run Data Item Type
1 Flow Time
2 Net Standard Volume Oil
3 Net Standard Volume Water
4 Indicated Volume
5 Gross Standard Volume
6 Average Temperature
7 Average Pressure
8 Average Density
10 Average Water Cut
11 Input Units
12 Contract Units
13 Alarm Count
14 Event Count
15 Meter Factor
16 K Factor
17 Meter Input Type
18 Average CTL: Oil
19 Average CTL: Water
20 Average CPL: Oil
21 User Data 1
22 User Data 2
23 User Data 3
24 User Data 4
25 User Data 5
26 Batch ID
27 Duration of period
28 QTR Identifier

Disclaimer

ClearSCADA 2017 R2