Source (Water Flow Run)

Associated with: SCADAPack Modbus Realflo Outsations, and SCADAPack Modbus Realflo Analog Input points

The Source attribute is common to many Status displays. The attribute indicates the location at which an item resides. The information shown varies, depending on the type of item.

For SCADAPack Modbus Realflo Outstations, the attribute displays information in this format:

Set <Set Address>:OS <Controller Address>

For SCADAPack Modbus Realflo Analog Inputs, the attribute displays information in this format:

Set <Set Address>:OS <Controller Address>:Flow Run <Flow Run Number>:AI Source <Source Number>:Item <Item Number> (Address <Point Address>)

where:

For information about either of the above properties, see Configure the General Realflo Analog Point Properties.

The table below indicates the type of Flow Run Source <Source Number > represents.

Source Number Source Type
0 Accumulation
1 Input
2 Flow Calculation
3 Compressibility Calculation
4 Density Calculation
10 Daily Flow History
11 Hourly History Data
12 Batch Records Data

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Accumulation (<Source Number>=0).

Item Number Water Flow Run Data Item Type
4 Net standard volume: water during previous contract day (Liquid only)
5 Number of flow calculations during contract day
6 Duration of flow during contract day
7 Gross Standard Volume at base conditions during contract day (Liquids only)
11 Flow duration in current month
13 Flow duration in previous month
15 Duration of flow during previous contract day
19 Number of flow calculations during previous contract day
22 Net standard volume: Water during contract day
23 Average temp correction factor: water CTLw current day (Liquids only)
24 Average temperature correction factor: water CTLw during previous day
28 Net standard volume: water during the current month (Water only)
29 Net standard volume: water during the previous month (Water only)

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Input (<Source Number>=1).

Item Number Water Flow Run Data Item Type
1 Calibration flags
2 Temperature Input Alarm
3 Static Pressure Input Alarm
4 Volume Flow (Liquid/Water) Input Alarm
4 Volume Pulse (Liquid/Water) Input Alarm
4 Mass Flow (AGA-11/Liquid/Water) Input Alarm
5 Live turbine meter pulses (AGA-7 or Mass/Volume Pulse AGA-11/Liquid/Water)
6 Live Temperature
7 Live Static Pressure
8 Live Volume Flow (Liquid/Water)
8 Live Mass Flow (AGA-11/Liquid/Water)
9 Forced Temperature
10 Forced Static Pressure
11 Forced Volume Flow (Liquid/Water)
11 Forced Mass flow (AGA-11/Liquid/Water)
12 Forced Pulse Rate (AGA-7 or Mass/Volume Pulse AGA-11/Liquid/Water)
13 Current turbine meter pulses (AGA-7 Gas or Mass/Volume Pulse AGA-11/Liquid/Water)
14 Current Volume Flow (Liquid/Water)
14 Current Mass Flow (AGA-11/Liquid/Water)
15 Current Density
16 Current Water Cut
17 Current Input Temperature
18 Current Static Pressure
19 Density Input Alarm
20 Water Cut Input Alarm
21 Live Density
22 Live Water Cut
23 Forced Density
24 Forced Water Cut

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Flow Calculation (<Source Number>=2).

Item Number Water Flow Run Data Item Type
2 Input or flow calculation result code
3 Flow volume rate
4 Flow mass rate
9 Date of Flow Update
10 Time of Flow Update

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Daily Flow History (<Source Number>=10), or Hourly History Data (<Source Number>=11).

Item Number Water Flow Run Data Item Type
1 Duration of Flow in Period
3 Net Standard Volume Water
4 Indicated Volume
6 Average Temperature
11 Input Units
12 Contract Units
13 Number of Alarms
14 Number of Events
15 Meter Factor
16 K Factor
17 Meter Input Type
19 Average T Correction (CTL) Water
21 User Data 1
22 User Data 2
23 User Data 3
24 User Data 4
25 User Data 5
26 Batch ID
27 Duration of period
28 QTR Identifier

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Batch Records (<Source Number>=12).

Item Number Water Flow Run Data Item Type
1 Flow Time
3 Net Standard Volume Water
4 Indicated Volume
6 Average Temperature
11 Input Units
12 Contract Units
13 Alarm Count
14 Event Count
15 Meter Factor
16 K Factor
17 Meter Input Type
19 Average CTL: Water
21 User Data 1
22 User Data 2
23 User Data 3
24 User Data 4
25 User Data 5
26 Batch ID
27 Duration of period
28 QTR Identifier

Disclaimer

ClearSCADA 2017 R2